Iv'e been reading the datasheet of BQ24140 (http://www.ti.com/lit/ds/symlink/bq24140.pdf, and there are a few issues which are not entirely clear to me:
1. What happens if both VBUS and VIN are connected to power and "CE" bit indicates on "active" in both?
2. How exactly does the "15min timer" work? If the device is connected to power and I2C communication only starts after more than 15min, will the device respond properly?
3. How exactly does the "32s watchdog" work? When is the dog kicked?
4. If both "CE" bits indicate "inactive", is there a possibility we'll enter a "deadlock" situation, in which the battery runs out and device will not allow any charging ever?
Thanks in advance!
Tal