This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A69-Q1: TPS7A6933 soft start feature

Part Number: TPS7A69-Q1


Hello Team,

the TPS7A6933 contains an internal soft start feature that reduces the current on the pass transistor during the startup. 

In regards to that circuitry I do have some questions, since the datasheet does not mention it explicitly:

The current limitation on the pass transistor is it limited for a fixed time or is it based on the input/output voltage threshold and can vary the time?

At which value is limiting (typical) the current?

Is it the Iout Imax 500mA typ. 800mA max?

Thanks,

SunSet