This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: Output Specs at Low Load (<10uA)

Part Number: TPS61099
Other Parts Discussed in Thread: TLV61224

I am planning on using the TPS61099 (3V fixed output version) with a single AA battery to power an MSP430 FRAM, an accelerometer (ADXL362), and a BLE radio (BLE113). While the ADXL is running the current consumption can be very low. I am curious what the output ripple and voltage accuracy of the TPS61099 is at very low output currents? Specifically at 1uA, 10uA, and 100uA. I know the inductor and capacitor choices impact this, so I plan to use the recommended the recommended circuit (1uH and 2 parallel 10uF with a 1uF).

Any help would be appreciated. Thanks!