Tool/software: TI C/C++ Compiler
I want to use TPS65835 ,but this IC only say MSP430x2xx in it .
which IC is in TPS65835 ? msp430F211 ,or msp430F212 .................
please tell me , Thanks !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
I want to use TPS65835 ,but this IC only say MSP430x2xx in it .
which IC is in TPS65835 ? msp430F211 ,or msp430F212 .................
please tell me , Thanks !
Yufei Huang,
The MSP430F2111 and MSP430F2121 are the same core. The only difference is the amount of memory and one or two options.
The TPS65835 has, 16 kB Flash Memory, 512 B RAM (More Memory)
The MSP430F2111 has, 2 kB Flash Memory, 125 B RAM
The MSP430F2121 has, 4 kB Flash Memory, 250 B RAM
The TPS65835 has both the 10 bit ADC and the comparator.
Start with the MSP430F2121 and use the design MSP430x2xx Family User's Guide, Literature Number SLAU144.