Other Parts Discussed in Thread: LM5170
I am Planing use the above given part number of IC for Power supply in automotive application. I want to use Buck and Boost mode with unidirectional. Input 30V to 80V, Output 48V fixed. Out put Current Max 420A at Peak power condition. Peak Power 20KW expected. How will control Output voltage of LM5170-Q1 IC. does it have inbuild feedback control or external voltage control loop circuit has to add. Could we use single IC or mutiple IC to meet required Peak Power Please advice for the same request