I want to confirm the pin setting when WDT is unsued.
When WDT is unused, set each pin as follows.
SENSE : connect to 3.3V
SET1 : connect to GND
SET0 : connect to 3.3V
CRST : onnected to GND via a capacitor(0.1uF)
CWD : open
VDD : connect to 3.3V
RESET : connect to reset of microcomputer
WDO : open
WDI : connect to GND
GND : connect to GND
note : The customer monitors 3.3V power supply.
Is this setting correct?
-Harukawa