Part Number: TPS63000
Other Parts Discussed in Thread: TPS63000, TPS63070
Hello,
I have a query below can you help?
Customer is seeing a couple of failures of the IC. The failure is occuring when the IC is starved of current. This pulls the input voltage down from 5V to approx. 2.5V and so the IC remains on (>1.8V Enable). The TPS63000 has an inrush current of ~1.4Amps.
Please could you tell me if;
- The soft start circuitry is optional i.e. do all designs using this TPS63000 require it?
- Is the soft start R3/C3 configurable, there is no mention of this in the datasheet?
- Can the device be damaged is starved of current?
- Have there been any similar reported failures?
The circuit is as follows. Depending on the supply, VIN could be 5V @ 500mA or 2A
VIN = 4.5V – 5.5V
VOUT = 5.2V
R1= 1M5
R2 = 160k
R3 = 100R
C3 = 100nF
C1 = 22uF
C2 = 22uF
L1 = 3u3H (LPS4018-332MRB)
will attach schematic shorltly, but would appreciate support in this