This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2845: Help check the schematic

Part Number: UC2845

Hi

Please help check the attached schematic.

Measure the gate pin voltage waveform of Q40, the voltage >30V chip no output.

Waiting for your reply.

Thanks

Star

  • HI Star

    What are the voltage waveforms on the gate drive pin 16, the Vref pin 9 and Vsense pin.

    What is the input voltage on the AC line? The oscilloscope picture shows a waveform, is that the gate drive when the input voltage is less than 30V?

    Thanks

    Peter