This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61096A: disable level shifters

Part Number: TPS61096A

Hello!

This device integrates power converter and two level shifters.  Also, this device has enable/disable function, controlled by EN pin.

Unfortunately there is no clear information in datasheet if EN pin controls this level shifters, no specification on enable or disable time. From other side, there is mentioned “Both level shifter channel enabled” in datasheet, and from this phrase I have impression this EN pin controls level shifter also.

So the question is: do level shifter also disabled by EN=low or this level shifters are always enabled?

With best regards, Yuriy