Hi , I see on the info page that the controller will do up to a 420A design. I have the EVM kit and it specify 180A . I do notice the power stages are either not out yet or special as there is no info on them. I was going to ask what is the absolute maximum the EVM will do, I know I can set limits out the roof but other than running it until it fails I don't know.
Thanks,