This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FInding a FET

Other Parts Discussed in Thread: CSD18502Q5B

Is there a part that matches the below description? 

(6 FETs, 3 Shunts, Thermistor)

Configuration 1

Shunts

0.5 mOhms

I_phase (RMS)

130A

V_DS for FETs

40V

FET approx typical Rds(on)

1.7 mOhms, (Vgs=10V)

Typical thermal resistance from FET junction to heatsink

< 2.0 degC/W

Thermistor

~4.7 kohm

Body 25mm x 60mm

Overall tip to tip on the leads 42.6mm

Signals out one side, Power input (Vbridge), phases

and GND on the other side

Lead Options

1.Leads with double bends as shown

2.  Signal leads single bend, power leads straight