This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO application question

Other Parts Discussed in Thread: TPS7A7200, TPS7A85, TPS7A85A

Hi Team,

I have LDO application question.

ANPEC device APL5950can support 5A (@0.15V drop voltage) and internal current limit up to 8A. package is SOIC(8) with power pad.
I calculate ANPEC maximum power dissipation up to 3W.( juction temp150 degree / 50 degree per watt).
if  output current 2A @1.5V drop voltage.

APL5950%2fA.pdf

Looks TI device. I not found same device compare APL5950, why?
I just can survey TPS7A7200??

  • Hi Kuo,

    We have a number of 5A devices and you can use the parametric search to find such devices: 

    http://www.ti.com/lsds/ti/power-management/single-channel-ldo-products.page#p451max=5;12

    If you only need 2A-3A then you can change the search parameters to show those devices:

    http://www.ti.com/lsds/ti/power-management/single-channel-ldo-products.page#p451max=2;3

    -Kyle

  • Hi Sir,

    You not answer my question, please help.
    I already survey TI device by web.

    Thanks!
    John
  • Hi John,

    Unfortunately I misinterpreted what your question was, I thought you were looking for help finding a 5A LDO. If you are looking for something more specific then we will need more information (such as key spec/functionality) to find a part that better suites your application. However, the parametric search contains all of TI's LDOs so if it is not there then we do not have it at this time.

    -Kyle
  • HI John,

    Maybe I can try to answer your question. The TPS7A7200 does have a nice low drop-out but this is rated at 2A. At 2A, the dropout when VOUT is <= 3.3V is only 180mV. For the same pass element, if the current limit allowed 4A, the drop-out voltage would be ~double this value. Our Flagship higher current LDO is the TPS7A85 which has a drop-out of only 240mV at 1.1VOUT.


    Another thing to consider in high current devices is the thermal performance. The TPS7A85 has a TJA of 35.5 C/W vs. the APL5950's TJA of 50/60 C/W depending on package. 

    Does this answer your question?

  • Hi all,

    Thanks for your help.
    last question. May I know general LDO design input 3.3VDC and output 3.15VDC/5A for what application? or just special function?
    looks ANPEC current limit 7A can shut down and thermal also can shun down(I guess when over loading)

    Regards,
    John
  • HI John,

    I am not aware of any applications that require 3.15VOUT. However, using any LDO in drop-out, there is no effective PSRR. While in Drop-out the pass element is fully enhanced so there is no real attenuation of any ripple on VIN.

    The most common application I have seen for high current LDO's is for DSP or FPGA VCORE power. These devices typically require precision regulation (i.e. <1% accuracy), and a fast load transient response. If you compare the Anpec device to the TPS7A85A, both have an N-Channel pass element so they both should have a fast load transient response. While slightly lower current. the TPS7A85A has Any-Out(TM) technology which allows you to set VOUT without external Feed-back resistors. This gives a real 0.75% accuracy over line/load/temp whereas the Anpec device's 1% accuracy does not include the tolerance of the external resistors required to set VOUT.

    Most high current LDO's that I have seen have current limit and thermal shutdown. Note: these protection solutions are present to protect the device so it can survive either a short or an application where the LDO is dissipating too much power

    I Hope this answers your question.


    Regards,

  • Hi Sir,

    Thank you!!

    Regards,
    John