This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Thermal shutdown of LP5907

Other Parts Discussed in Thread: LP5907

I have a question about LP5907.

Thermal shutdown threshold is 160℃.

Please tell the reason why threshold is 160℃.

I want to know the basis of 160℃.

Best regards,

Takahiro Nishizawa

  • Hi Takahiro,

    The thermal shutdown threshold is set at 160C for a variety of reasons. A few examples include:
    1) Package handling temperature. Some plastic packages suffer degraded reliability quickly once the case temperature gets into the 170C+ region. 160C provides margin from that area
    2) Solder. Leaded solder melting point is ~180-190C, so again the 160C provides margin from keeping the temperature away from that away
    3) Device operation. A lot of variables in silicon-based device models start to turn non-linear in as the temperature gets significantly above 160C. An example is leakage currents - they get exponentially larger at high temperatures. These variables can cause abnormal device operation.

    In summary, a lot of factors play into why thermal shutdown is typically kept near 160C.

    Regards,
    David