Other Parts Discussed in Thread: LM3450, LM3409
IN THE PRESENT APPLICATION, THE LM3450 EVALUATION BOARD WILL "SEE" AN 120VAC INPUT WHICH WILL BE 'TRUNCATED' DOWN TO 15V rms. THE SOURCE AC WAVEFORM IS FROM A TRIAC CONTROLLER. THIS IS USED TO DIM A SET OF PARALLEL LED DRIVERS. THE DOCUMENTATION I HAVE FOR THE LM3450 BOARD DOES APPEAR ALLOW FOR AC INPUTS OTHER THAN THE USUAL SINE WAVE FORM.
IF THE LM3450 IS NOT SUITABLE HERE, PLEASE RECOMMEND A LED DRIVER PRODUCT WHICH IS DIMMABLE BY THE AC INPUT
DAVID W ROGERS PE