This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24070: Running BQ24070 Devices in Parallel

Part Number: BQ24070


To gain additional output current capacity, I want to connect four of these devices in parallel. Each device would have the same input voltage source, and connection to the same high-current battery. The status and control signals would be managed separately for each device. The output of each device would be independent and isolated.

Is this possible to do?

Thanks,

                        Damon