Hello,
There are some questions during BQ24773EVM test as below.
-. Do I have to use TPS3898ADRY(U2) for BATPRES or can remove it to use internal comparator?
-. Set S1 switch as 1 & 2 close, 3 & 4 open to use internal comparator, BATPRES LED is ON without Battery.
-. Is there anything to set to use internal comparator?
-. According to EVM BOM, all resistors' tolerance is 1%.
-. Can I use 5% resistors instead of 1%?
-. During charging test, D2(BAT54C-7-F) goes to fail. Could you let me know the maximum current of D2 when battery charging?
-. Let me know why this Diode goes to fail?
-. If I don't want to use Vsys Out, how can I treat SRN/SRP pin?
-. All components for Vsys can be removed?
-. Could you let me explain the purpose of Q1A & Q1B on EVM?
Regards,
Nicky