Other Parts Discussed in Thread: TUSB321AI, TUSB422
Hello
We integrated the 5A Li-Ion charger BQ25890H in the power management of our USB-C device for fast charging Li-Ion batteries with maximum 5A. As a power source we tested a USB-PD power adapter, but it does not work. We do not get any voltage at the USB voltage pins. Other USB-C adapter (Quickcharge 3.0 or 3A 5V charger with USB-C connector) work fine. I assume there is a problem with the hand shake. My questions to you:
- Does the BQ25890H support USB-PD yes or no?
- If no, is there a pin compatible version of TI which supports USB-PD and does not require a redesign of the hardware?
- If yes, can someone help us with the right handshake?
Thank you for your support.
Felix