Hi,
I am looking for a DCDC for automotive use.
The specification is below.
VIN: 5.5 V to 18 V (40 V load dump)
VOUT: 5 V
IOUT: 30 mA typ, 60 mA max
SW frequency about 2 MHz (I want to operate at 2 MHz even at 30 mA)
The PeakLimit current should be lower, because VIN is a lead battery
I found LMR 16006 Y-Q1.
I would like to check a few things about this device.
The figure below is excerpted from the data sheet.
I want to operate this device at VOUT = 5 V when VIN = 5.5 V. I judged it as possible from the figure, but is it correct?
At this time, can it operate at 2.1 MHz?
Best Regards,