Hi,
I am looking for a DCDC for automotive use.
The specification is below.
VIN: 5.5 V to 18 V (40 V load dump)
VOUT: 5 V
IOUT: 30 mA typ, 60 mA max
SW frequency about 2 MHz (I want to operate at 2 MHz even at 30 mA)
The PeakLimit current should be lower, because VIN is a lead battery
I want to check if TPS 57040 - Q 1 meets specifications.
I understand that this device turns off when the voltage of the BOOT capacitor drops below 2.1V.
However, I do not know what the maximum duty cycle is.
In my specification, 91% DUTY is necessary.
Please tell me the maximum duty of this device.
Best Regards,