Part Number: LM2577
Other Parts Discussed in Thread: LM5022, LM25118
I've seen modules boards (in ebay) with LM2577 used as buck-boost. I don't see such aplication in the datasheet. It is possible to use it like that?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you both for your answers!
I should have been more clear about our application. Also, switching supplies it is not something I feel very comfortable with, so bear with me.
We have an input wich goes from 8 to 16V and we want a 12V output, At first we thought 1A would be enough and we were using an Linear Tec part (LTC3114-1). We had some issues with that part (mainly for the lack of experience with DC-DC converters) and we couldn't reach anywhere near 1A.
Now we are looking for something that could deliver more current (at least 2A) but something easeier, simpler, something like "DC-DC for dummies" :) .
We found this LM2577 based buck-boost converters and they look simple enough to be replicated in our application. I found an schematic for the modules (see attach).
1-Would you say is feasible to reach 2A?
2-How would you chose the components value to do that?
I also found out that what we are looking for is a "SEPIC" and knowing that I found the application PMP7768 that uses an LM5022. That circuit would satisfy our needs but I would prefer a low count parts solution with a LM2577-12 if it is possible.
Thanks again!
Hello,
SEPIC converters can be very complicated to design and parasitics can drastically change the performance of the converter. That being said PMP7768 would be a good starting point for this application. HEre is an app note that goes through the basic operation of a SEPIC converter. I would suggest using the LM5022 over the LM2577 as the LM5022 has a selectable current limit threshold as the LM2577 is a fixed current limit.
The other option is to use the a true buck-boost controller, like the LM25118. This can be a much simpler design as is only requires 1 magnetic which reduces the impact of parasitcs in the design. However the LM25118 will require two MOSFETs and two diodes. This is another good option for a buck-boost controller that should be easier to design than most SEPICs.
Please let me know if you have any questions.
Thanks,
Garrett