Other Parts Discussed in Thread: BQSTUDIO, , BQ34Z100
I am using a EV2300 board to program a bq34z100EVM board. I open up bqstudio and it auto-detects my device and starts up fine. Then information on the right hand side is not grayed out and I am able to communicate with the device using the commands on the right hand side. Then I go to set the ChemID and I keep getting "Error code = 3" 90% of the time and "Error code: 1470" 10% of the time. I have attached screen shots of the error messages. How can I set the ChemID?!?!?