Hello My friends .
Im working on a project using lm5008 to produce 12 volts . My input voltage varies between 16 to 60 volts. The IC internal current limit works good and disconnect the circuit in overload and short circuit When the input voltage is low (16 to 36), but when I increase the input voltage , and increase the load in high voltage , The IC breaks and burns.
When I increase the load step by step when the input voltage is 60 volts , suddenly the output voltage rises and then the IC breaks,
This is my circuit :
This picture is the sw pin and output when the load is 40 Ohms (300 mA)
And this is the sw pin and output when the load is 20 Ohms (600 mA)[I expected the circuit be off in this current].
Please Help me.