This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: In the application below, I'm thinking about what to do with load switch with input reverse polarity protection.

Part Number: TPS2660
Other Parts Discussed in Thread: LM5060, TIDA-01167

Thank you for your patronage. 

In the application below, I'm thinking about what to do with load switch with input reverse polarity protection.

I intend to use the LM5050 or LM5060 or TPS1H100 or TPS1H 000 for the load switch IC on the Vin side.

But I can not find the load switch IC on the Vout side. I know that there are TPS 2660 and TPS 25927 as load switching ICs with input reverse polarity protection. But they are not suitable for my application because Vout, Iout reach the Absolute Maximum Rated value. 

I am not stuck with using load switch IC. I am also considering driving load switches with discrete parts. However, it is difficult for me to drive the load switch with discrete parts. 

A method that costs as low as possible is good.

Could you give me some hints? Thank you.