This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62743: Review my Schematics.

Part Number: TPS62743


Hi All,

I attached a file that is schematics of TPS62743

VBST : 5V / 50mA

VDD_M : 3.3V / 80mA

M_PWR_CTR : 1.8V 

That is for Wearable Device.

Review my schematics , ASAP.

Best Regards,

Inho Jeon.

TPS62743_SCH_1.pdf