Other Parts Discussed in Thread: , MSP430G2553
Dear TI,
I'm developing power injector with 4-pairs(2x2 pair 45W) using TPS23861 Single-port.
-Spec (10/100/1000 Data Rates)
|
Class |
Type |
#Pairs |
Power Sourced at PSE |
|
5 |
3 |
4 |
45W |
I intend to develop using 2-Ports. Is it possible?
Also, do you need an additional MCU to be compatible with Endspan and Midspan?
If there is no MCU in the 2(PSE) x 1(PD) solution, the 2 PSE will perform detection and classification at same time.
Thus, the detection and classification not conflict?
Do I need an external 3.3V power to drive the TPS23861?