Other Parts Discussed in Thread: BQSTUDIO
Hi,
I'm using the BQ34110 with an external voltage divider (two 100k resistor). The max battery voltage of the system is 4.5V.
The control of the BQ34110 is done with a microcontroller via I2C interface. I'm trying to read the battery voltage but still reading 0V.
I've send the I2C command to put the bq34110 in CAL mode (Calibration mode) and set the VEN_EN bit at 1.
Here is a picture of the VEN output that enable my voltage divider to the bat input of the bq34110.
Here is a picture at the BAT input:
I should be reading 2.2 V and I read 0 V. I don't understand why.
Thank you!
Michael