Hello
One of my clients is using the TPS548D22RVF for this project.
It seems to me that it was applied with the right design values.
Could you please take one more review?
I will deliver the corresponding schematic file.
<< schematic deleted >>
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
One of my clients is using the TPS548D22RVF for this project.
It seems to me that it was applied with the right design values.
Could you please take one more review?
I will deliver the corresponding schematic file.
<< schematic deleted >>
Hello Andy,
Please make the following changes:
1. Zero Ohm resistor in series with C94.
2. Snubber circuit as place holder at SW node (470pF + 3.01 Ohm).
3. C99 as no pop or delete it.
4. EN_UVLO R31: this pin has maximum rating as 7.7V. Concerning the ringing voltage on the input voltage can damage this pin. Suggest to have a resistor divider on this pin.
5. ILIM R35: this value gives about 45A OCP. What is the customer limit value? Please see Figure 15 on page 13 for details.
6. Input capacitor: seems not enough to cover the RMS value. Please verify the capacitor manufacture datasheet.
Hello
Thank you for your reply.
I'm curious about the changes you've made.
1. I want to know why I connect 0OHM in series with C99.
3. I want to know why I removed C99.
4. The input voltage of this circuit is 5.6V. UVLO The internal pressure of the PIN is not exceeded.
If so, should I add a resistor?