This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23630: inverting buck converter reference design

Part Number: LMR23630

Hello,

Our customer using LMR23630AF as their standard buck DC/DC IC.

Now, they are trying to build inverting buck converter with LMR23630AF,

however, webench tool cannot make that circuit yet, so they want to know any other way to design their circuit easily.

When can we simulate inverting buck converter with LMR23630 in webench ?

Or, could we have some reference design with LMR23630 as below conditions ? 

input : 5V,  output : -15V, 1.5A

Thanks and best regards,

Hiro