Part Number: LMR23630-Q1
My customer would like to apply the LMR23630-Q1 and modify only the Rfbt value to change the output.
Vin : 25V / Vout : 5V or 3.3V(Modify the Rfbt) / Iout : 3A
Cout and Lout proposed calculating the minimum value in the datasheet and applying an integer higher than that value.
But I do not know how to suggest Cff.
Datasheet is shown in "CFF is not needed when COUT has very high ESR and CFF calculated from Equation 19 must reduced with medium ESR.".
If I use a high ESR alu-cap, do I not need CFF?
If I use a low ESR Ceramic CAP, do I must need CFF?
If I use a small CAP with ESR and do not apply Cff, what kind of problems will I encounter?