This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM53635-Q1: Vout max limit for LM53635

Part Number: LM53635-Q1

Hi,

I found the Vout max is 10V. I would like to know why it has this limit? Can I have any chance to design a 15V output?

Thanks.

  • Hello,
    Yes, you can design this device for an application with output voltage >10V.
    However , if designing for an output of 15V, designer needs to ensure that minimum off time specification is not being violated.
    Also passive components (L, Cout, feedback divider etc) values would have to be calculated and adjusted accordingly.
    regards
    Brani