I am using a bq40z60 gas gauge in 4S configuration. Batteries are Li-Ion NCR18650B (Chemistry ID 2012).
Now I run a learning cycle on one board and after that set Update Status to 02 and Cycle Count to 0. If I use this Golden file on another board in production that has imbalanced cells (e.g 3800mV, 3800mV, 3800mV and 4300mV), will the bq40z60 on the second board balance the cells without generating Safety Alerts/Statuses during charge/discharge?
Thanks!