Hi,
I am using the bq27621-G1 in an application where the battery is not removable from the system. This design is also extremely space constrained: 0201 size components used throughout the design.
I am not using GPOUT in the application. Our programming model will never put the gauge into shutdown power mode. We are not using GPOUT for detecting gauge status.
In the datasheet, there is note that even if GPOUT is not being used, it SHOULD not be left open and it is recommended to pull it to VDD through a 10K resistor. If the datasheet said ".... MUST not be left open ...", I would not be asking this question.
My question is why is this pull-up required?
I have the bq27621 EVM board and have it configured so that GPOUT is floating. I don't see any erroneous operation in this configuration.
Regards,
Todd