Other Parts Discussed in Thread: BQ24735
Hello,
Regarding to the short circuit protection on BQ24780S,my customer is asking some question.
They are using BQ 24735 on their application and they will use BQ24780S on new product.
(Question)
(1) About short circuit protection registers on internal FET,
<BQ24735>
IFAULT_HI:ChargeOption[8] POR 750mV
IFAULT_LOW:CahrgeOption[7] POR 135mV
<BQ24780S>
HSFET VDS Threshold(IFAULT_LOW):ChargeOption3[7] POR Disable
LSFET VDS Threshold(IFAULT_LO):ChargeOption3[6] POR 250mV
They will use as POR on BQ24735 and will use as POR on BQ24780S similarly.
Also they will use default value in IFAULT_HI/LOW on BQ24735,
and will use default value in HSFET/LSFET VDS Threshold on BQ24780S similarly.
In this case, is there any problem or concern?
Regards,
Tao2199