Hello,
I need to extend the cycle-by-cycle current limiting beyond the time set by the soft start capacitor. Specifically I need to stay in cycle-by-cycle current limit until the output voltage drops to 30% of nominal. I have an idea to clamp the ss pin to 4.3V until the output voltage drops to the required value. Once it reaches the 30% of the nominal voltage I remove the voltage clamp from the ss pin and allow it to go into hiccup mode. Does this sound feasible?
I am asking because the TI data sheet is somewhat vague about its description on how the UCC28950 current limiting works. For example, the data sheet says that the time allotted for the cycle by cycle current limiting is set by the soft start capacitor and the discharge current, Ids. But the soft start capacitor also sets the soft start time. This makes it difficult to meet the standard specification I mentioned above.
Has anyone tried extending the cycle by cycle current limiting?