Other Parts Discussed in Thread: UCC28631, UCC28630
Hi all,
Is it possible to use UCC24612-1 as S.R. for UCC28631 CC mode ?
www.tij.co.jp/.../ucc24612.pdf
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Is it possible to use UCC24612-1 as S.R. for UCC28631 CC mode ?
www.tij.co.jp/.../ucc24612.pdf
Thank you!
Bernard-san,
My concern is rapidly load increase <--> decrease.
Like this increase -> decrease -> increase-> decrease rapidly.
Is it OK ?
If it is ok, W/W input 160W output with high efficiency can be acheaved?
Thank you,
H.DOI
Doi-san,
The Flyback stage will behave in the same way with with diode or SR when the load increases into CC region and then back to CV region - there should be no difference.
Here is a plot of the load step from 40-ohm (~0.5 A) to ~2.2-ohm (limited in CC mode to ~7 A, hence Vout drops to ~15 V), then back to 40-ohm.
This was measured on UCC28630 EVM, modified with SR + UCC24612-1; (red is Vout, pink is Iout):
However, there is one area that is affected by the SR driver - when the Fsw drops very low as load is decreased to a very low level, the SR driver stops driving the SR gate, then the SR FET body diode rectifies. The increased Vf drop causes Vout to regulate ~0.5 V lower at standby/no-load.
At a certain range of load, where Fsw is close to the SR driver light-load enable/disable thresholds, the operating made can repeatedly cycle between SR driving and not-driving, causing Vout to cycle up & down by ~0.5 V (body diode Vf drop). On the EVM, this is seen at ~50-100 mA load range.
Note that this is only happenning because of the PSR controller on the primary - the Vf drop change looks like a step-change in Vout and causes the primary loop to react accordingly. This would not be seen with SSR/opto feedback.
Thanks,
Bernard