This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54625: can't power up

Part Number: TPS54625


see schematic below.

  1. after power on,VOUT is 0.8V.
  2. The wave shows Vin (blue 12V) shakes at rising edge.
  3. Vout (yellow 2.5V) ends below 1V.

why tps54625 can't retry and get back to work normally?