Hi,
my job is to design a BMS for a 12s3p cell pack, but I am pretty new to this and kinda overwhelmed by the possibilities. The cells which will be used are NCR18650B and I want to monitor current, voltage and temperature of every cell. Balancing will be passive.
There is not much space for the BMS board, so every function should only be there one time. The problem is that the charger ICs I've seen already have a monitor function implemented. Do I even need a charger IC or can I implement it via software if I use a gas gauge? Would there be drawbacks?
Is it better to measure all 12 cells in series with one IC or are there advantages e.g. for design if I split up the monitoring to 6 cells or so per IC?
Best regards