TPS54160 team,
We have a customer using TPS54160 who needs to delay the rise of the output voltage. Input is typically 45VDC. Output is 12VDC. As the input gradually rises past 26VDC, they want the output voltage to rise 700 ms after the input passes 26VDC. It's a delayed start rather than a slow start.
Would you recommend some sort of delay circuit implemented on the EN pin, or is there a creative way this should be done with the SS feature (Slow Start / Soft Start)? Do you have any example circuits?
Thanks,
Darren