Hi,
My query relates to the EMB1499/EMB1428 active balancing solution.
Specifically, the EMB1499 bidirectional forward converter.
I’m having doubts as to the component selection guidelines. The reference design for this solution has component choices that contradict the guidelines in the datasheet.
Links to relevant documentation below:
Reference design schematics: http://www.ti.com/lit/pdf/tidrn59
Reference design BOM: http://www.ti.com/lit/pdf/tidrn60
EMB1499 datasheet: http://www.ti.com/lit/gpn/emb1499q
The first issue relates to the forward transformer selection.
The datasheet specifies the following:
- Turns ratio should be n:1 where n = 0.25 * num_cells
- Primary side inductance minimum 190uH
However the reference design uses this Pulse part (T1 on schematic and BOM):
which is only 128uH and the max turns ratio achievable is 3.14. Note that this is for a 16 cell design, so the ratio should be 4:1.
Your thoughts?
Thanks.
DJ