This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: Constant - very wrong - cell measurement

Part Number: BQ76930


Hi,

We are having trouble with the BQ76930 chip reading and reporting completely wrong cell measurements, ranging from 0.7V to 24V. This error has occurred on 3 different chips on 2 different boards, and is based off the raw ADC value read by a logic analyser on the I2C-path (i2c read/write, including alerts, with host works as expected). All 3 chips report the same values, and does so immediately after first power on, without any balancing, chg on, or dsg on. We are at a loss as to why this is happening, considering an earlier revision of the same board, without any changes to the AFE, works without problems. The only change is an added host µc drawing power from REGOUT pin; could this damage the BQ-chip somehow? Power drawn should not exceed 30-40mA.

The system is 10 cells at 3.8V, with BQ76930 as AFE and nRF52 as host µc.

I have attached the schematics and board layout, as well as a log of reported cell voltages (adc values, decimal). Any help noticing errors would be greatly appreciated! If any other information is needed let me know.

7840.1.pdf

5086.2.pdf

Cell 1    Cell 2    Cell 3    Cell 4    Cell 5    Cell 6    Cell 7    Cell 8    Cell 9    Cell 10
3425      3108      9468      32116     9970      62917     9970      62658     10229     13954
3425      6479      9468      33941     9970      62917     9970      63969     10229     14213
3425      3885      9468      31859     9970      62917     9970      62658     10229     13954
1616      53808     0         4734      9970      49481     9970      60813     10229     12432
1616      53808     0         4734      9970      64232     9970      60813     10229     12432
3425      2614      9468      27651     9970      62917     9970      62658     10229     14213
2676      47663     9468      31590     9970      62658     9970      62658     10229     13954
3174      47137     9468      31859     9970      62917     9970      62658     10229     13954
1616      53561     2104      31590     9970      61060     9970      60554     10229     12237
1616      53561     2104      31590     9970      61060     9970      60554     10229     12237
3425      0         9468      30277     9970      62917     9970      62658     10229     13954
3425      3108      9468      32381     9970      58546     9970      62658     10229     14213
3425      4208      9193      2614      9970      62917     9970      62658     10229     13954
1879      2865      2104      46085     9970      61060     9970      60813     10229     11460
3174      44611     2104      46085     9970      61060     9970      60813     10229     11460
3425      3885      9468      32381     9970      62917     9970      62658     10229     13954
3425      3626      9468      32116     9970      62917     9970      62658     10229     14213
3425      3626      9468      32116     9970      62917     9970      62658     10229     13954
1616      52589     2104      31590     9970      58546     9970      60813     10229     12432
1616      52589     3108      26165     9970      58546     9970      60813     10229     12432
2931      38370     9468      32116     9970      62917     9970      62658     10229     13954
3174      53091     9468      31590     9970      62917     9970      62658     10229     13954
3425      4471      9468      32905     9970      62917     9970      62658     10229     13707
1616      54565     2104      32634     9723      52589     9970      51318     10229     12237
1616      54565     2104      32634     9723      52589     9970      62658     10229     12237
3425      1554      9468      31329     9970      62423     9970      62658     10229     13954
3425      2367      8416      28173     9970      62917     9970      62658     10229     13954
3174      26418     9468      33166     9970      62917     9970      62658     10229     14213
1616      54565     2104      32634     9970      61315     9970      60813     10229     12432
1616      54565     2104      32634     9970      61315     9970      60813     10229     12432
3425      777       9468      32381     9970      62917     9970      62658     10229     14213
3425      4471      9468      32905     9970      62917     9970      62658     10229     14213
3425      3626      9468      33166     9970      44362     9970      62658     10229     13954
1616      55083     2104      46603     9970      59793     9970      60813     10229     12432
1616      55083     2104      46603     9970      59793     9970      60813     10229     12432

  • I've experienced a similar issue, though, it seems like my IC is being slowly damaged over time since the voltage measurements are accurate for a little while after I first assemble a board. Eventually I begin to notice inaccurate readings from the BQ IC. I'm not drawing any current from REGOUT (just a 4.7uF cap to ground).

    Any insight into this would be greatly appreciated!
  • Some minor progress; connecting Bat/Pack - and +, as well as DSG and CHG to the battery (previously only the cells were connected, VC0-10) stabilises the cell readings, however they are still wrong with every other cell being wrong. See table below (~10k is correct, 0.5k/64k is wrong):

    Cell 1 Cell 2 Cell 3 Cell 4 Cell 5 Cell 6 Cell 7 Cell 8 Cell 9 Cell 10
    10167 526 9970 63969 9970 64232 9970 63969 10229 15265

    Pack voltage is however read (more or less) correctly at 24930 (ADC; real value 38.2V).

    Are there any known issues that could result in this pattern?