Other Parts Discussed in Thread: BQ40Z50-R1
Hi,
I look at the two specifications of the reference circuit,found the following problem, can help solve?
1.BQ20Z50-R1 have two resistance with SMBC and SMBD,respectively 100Ω and 200Ω. But BQ40Z50-R2 have only one resistance with SMBC and SMBD,it is 100Ω. What is the reason for this?
2.BQ40Z50-R1 have two capacitance with SRN and SRP,I think is optimization of detection. But BQ40Z50-R2 cancel this design.What is the reason for this?
3.datasheet Page 1,FUSE pin have a diode,but reference circuit cancel this design.What is the reason for this?
As shown in the figure below:
BQ40Z50-R1
BQ40Z50-R2
DATA SHEET PAGE 1--FUSE PIN