Other Parts Discussed in Thread: BQ24040EVM, BQ24040, BQ51013B,
I have a bq51050BEVM-764 (HPA764 Rev C) module. And want to test it with external power adapter as mentioned in "9.2.2 Application for Wired Charging" of the datasheet using bq24040EVM. But in the datasheet of bq51050BEVM, it says " adapter option is not supported in this HPA764-002". On the EVM, the FETs Q1 are not soldered and BAT is directly connected to J3 (OUT).
It seems I cannot connect the bq24040EVM even if I add Q1 on bq51050BEVM because BAT is directly connected to J3 (OUT) bq51050BEVM. Is there way I can test these two EVMs together?