Hello
We are using the BQ34Z100-G1 as the fuel gauge in a Li-Ion battery management system.
Our test team have reported that the fuel gauge is slow to report current at low values - it can take up to 30 seconds to report when current is less than 10A.
Current reporting is instantaneous at higher currents (i.e. 30A).
Our Micro-controller firmware interrogates the fuel gauge once every second, which I believe to be the maximum refresh rate of the fuel gauge.
Can anyone suggest what the cause of this issue may be?
Thanks
Dan Farrelly
Hyperdrive Innovation