This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54527: Component selection inquiries

Part Number: TPS54527

Hello,

I have two questions - one which is related specifically to the TPS54527, and the other more general.

1. In the TPS54527 datasheet, under the "Typical Application" section, there is a 10K resistor connected to the EN pin. Why is that? What is the rationale behind this?

2. For example in the TPS748, under the "Application Information" section, there is a table, listing different output voltages and corresponding configuration resistor values. However - in some cases, the theoretical value of the output voltage one gets from calculating using the 0.8*(1+(R1/R2)) formula deviates from the stated output voltage in the table. This deviation is, however, very small. What is puzzling though, is that "perfect" voltage is achievable using common resistors. For example:

  •  The table states, for example, the following resistor combination for 1.2V output - R1=2.49K R2=4.99K. Calculating using the formula yields 1.1975....V output. ~2.5mV deviation.
  • But, it is possible, while using "Standard 1% Resistor Values", to get exactly 1.2V using R1=1.1K and R2=2.2K. These even are more "common" resistors, much more available if you are a hobbyist. These resistors are still fulfilling the R2 smaller than 4.99K suggestion in the datasheet(if smaller currents required, 1.8K and 3.6K also work).

This phenomenon is seen across many datasheets in similar sections, across different manufacturers and different parts. It seem that there is some advantage in using E96 resistors even if the configuration is slightly off, while the E24 series gives perfect results(and are widely available in 1% tolerances).

Now, i am a novice, and it seems i am missing something that is perhaps obvious to anyone in the industry dealing with such components - why most datasheets recommend using values that yield an imprecise voltage, while more common, more precise resistors are available? 

Thank you,

Shay

  • In the TPS54527 Datasheet, the 10K is used to limit the current to protect the EN pin from damaging by huge current . you also can use a 100K to connect with the EN pin, but the big resistor means more noise.

    For the FB pin we usually use the resistor in 1% tolerance.

    The TPS748 is not our team's part, you can change the part number to get more detail about the TPS748. Thank you!

  • Thank you, but i cannot find in the datasheet of TPS54527 any mention of maximum current through the EN pin, Is it there to protect the device beyond the absolute maximum voltage on that pin? if so, can it be omitted if voltage on EN is guaranteed to be within operating range?
  • Yes, make the voltage of EN is less than 20V and connect a 10K resistor to limit the current. The EN logic is just a comparator.