I wish to modify the LED indicating thresholds in bq40z60 Golden image file from the defaults of 25%, 50%, 75%, and 100% to 15%, 50%, 75%, and 95%. What is the easiest way to do this? Can I just edit the file? Is there a checksum involved that I have to worry about. Please tell me the fastest and easiest way.