Other Parts Discussed in Thread: MC33063A
I am in need of clarification, the datasheet states on page 11 figure 12 shows a different value for the input than listed in the power supply recommendations
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Devon,
Figure 12 of the datasheet is a layout recommendation (pg17). Can you please attach an image of the figure you are referring to?
Here is the link to the datasheet that I am looking at.
Thanks,
Garrett
Garrett,
The design is configured as a buck converter.
The end-use of the device MC33063A is as follows:
1) input supply range from 9V to 30V
2) output is 5V
3) load is up to 700mA, with 500mA typical.
What is the recommended input side decoupling capacitance? 300uF appears to be adequate. 100uF is not enough, too much back emf is getting to the PS.
What is the recommended output load capacitance? 440uF is on output. There is still some ac ripple (150mv) on the output and is also not filtering HF noise being coupled from another switching circuit in the system.
Please get back to me as soon as possible.
Thanks,
Clinton
Clinton,
In a buck converter the input capacitance must be larger when compared to a boost because the input current is discontinuous. Based on your application 300uF seems reasonable. If you are worried about conducted EMI the capacitor should be larger, or an EMI filter can be added to help reduce high frequency EMI. Here is an article about designing an EMI filter.
The output capacitance of the buck converter is based on the amount inductor current ripple and the amount of allowable output voltage ripple. This is really independent of IC selection and is based on the design parameters. This application note will walk a designer through some of the more common calculations for a buck converter. 400uF seems like it should be adequate for this application. HF frequency noise can be eliminated by adding ceramic capacitors to the output and can also be impacted by board layout and how the signal is probed. Here is blog that walks though some of the steps for reducing high frequency output noise.
Thanks,
Garrett