This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54233: Soft start time: 1 mS>

Part Number: TPS54233

ello.

I have a question about TPS54233.

In the data sheet, the soft start time is specified in the range of 1 mS - 10 mS. Why is this?
I want to make soft start time 1 mS or less.
Is there a problem?

thank you.

  • The ss time set between 1ms to 10ms to ensure good start-up behavior.
    The frequency of this part is very low(300KHz), If the ss time is very short , the output could not start up well because of the low switching frequency (300KHz). Even if it can start up ,the output ripple during the startup will be big.