This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: About WEBENCH

Guru 21045 points
Part Number: TPS65131


Hi Team,

 

I can’t simulate TPS65131 at the following conditions.

-VIN=3.15V

-VOUT1=+5V / 0.8A

-VOUT2=-5V / 0.4A

 

According to Figure2 and 4 of the datasheet, I understand I can use TPS65131.

Is this a bug of WEBENCH?


 

Regards,

Kanemaru