Hello,
I'm looking for a LED driver from TI for following specicfications:
7 strings of 5 LED's each (total 35). Current through each needs to be 350mA.
Input DC voltage is more or less equal up to 24 Volts. As a result I need
a LED driver with 18V output voltage (forward voltage 3,6V each LED)
and a total current load of 2,45A.
Searching for driver I found the "TPS61086". Is that the right driver for my application ?
Regards,
Michael