Hi,
I have designed an OTG power bank using BQ24295. I am using the default mode of operation. Following is my circuit for reference. But when I try to charge an external device, I get a default charge current of not more than 500 mA at the PMID pin. According to the datasheet, the default current should be 1.5A. I don't seem to understand where does the problem lie.